Conry received the award Feb. 12 at the IOR Annual Dinner in London.
Conry designed from scratch a compressor that would meet all of the refrigeration industry’s needs for the future, based on his own extensive experience in the field of chiller and compressor rebuilding and maintenance. He assembled a world-class international team of experts with a mission to develop a centrifugal compressor that would operate at high variable speeds, be extremely efficient, oil free, lightweight, quiet and cost competitive.
“Having spent 15 years getting the compressor to where it is today, receiving this prestigious award really is ‘the icing on the cake,’” Conry said. “It is a privilege to be recognized in this way.”
In order to commercialize the compressor, in 2004 Turbocor entered into a joint venture with Danfoss and formed Danfoss Turbocor Compressor Inc. To date, over 10,000 Turbocor compressors are now in operation worldwide. Conry continues to develop this technology to achieve even further efficiencies and newer models.
About Danfoss Turbocor Compressors
In a new world of deregulating energy markets, environmental focus, and converging technologies, Danfoss Turbocor's mission is to redefine lifetime operating costs for commercial HVACR applications. The enterprise is dedicated to the design, manufacture, marketing and support of the world's most efficient commercial refrigerant compressors. The result is the world's first totally oil-free compressor specifically designed for HVACR. With its breakthrough convergence of industrially proven component technologies largely sourced from the aerospace industry, Turbocor's compressors promise new horizons in energy efficiency and lifetime operating costs for mid-range chiller and rooftop HVACR applications.
For information visit Danfoss Turbocor's website below.